Data Fields |
|
struct { |
| uint32_t OverWriteEn:1 |
| uint32_t LeftAligned:1 |
| uint32_t ScanModeEn:1 |
| uint32_t CTUEn:1 |
| uint32_t AutoClockEn:1 |
| uint32_t EOCTUIsrEn:1 |
| uint32_t JEOCIsrEn:1 |
| uint32_t JEOCHIsrEn:1 |
| uint32_t EOCIsrEn:1 |
| uint32_t EOCHIsrEn:1 |
| uint32_t DMAClrOnRead:1 |
| uint32_t DMAEn:1 |
| uint32_t ClkSel:1 |
| uint32_t Reserved:3 |
| uint32_t LatchPhaseDuration:1 |
| uint32_t Reserved0:1 |
| uint32_t OffShiftConfig:2 |
| uint32_t Reserved1:1 |
| uint32_t ComparisonPhaseDuration:2 |
| uint32_t Reserved2:1 |
| uint32_t SamplingPhaseDuration:8 |
| } | P |
|
struct { |
| uint16_t Mixed |
| uint16_t CTR |
| } | R |
|
uint32_t | W |
The documentation for this union was generated from the following file: